Kinetis Power Estimation Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Power Estimation Tool

6,963 次查看
stank
Contributor I

Hi,


I just downloaded new Power Estimation Tool for Kinetis, but after installation, I cannot select any Series or MCU.

Did anyone already test this tool?

 

Thanks,

Stan

标签 (1)
标记 (1)
0 项奖励
回复
8 回复数

6,048 次查看
_daniel_
Contributor II

Hi! Does anyone have a download link that works? Thanks.

Kinetis® Power Estimation Tool|NXP 

https://cache.nxp.com/downloads/en/calculators/Power_v1.0.1.exe?__gda__=1499303906_6a5146852f5c849af... 

The download link result in Page not Found.

0 项奖励
回复

6,048 次查看
rinipatel
Contributor III

I had the same problem on Windows 7 PC behind the proxy. It was resolved by modifying the kpet.bat as below (if you don't want to enter proxy ip and port settings manually):

start  jre/bin/javaw -Djava.net.useSystemProxies=true -Dcom.freescale.restapi.server=http://kex.freescale.com -jar mainWwin32.jar

Thanks,

Rini

0 项奖励
回复

6,048 次查看
marcusbainbridg
Contributor I

I had this problem on a PC behind a firewall/proxy.  It seems the java program doesn't system proxy settings.  TO force a manual proxy, in kpet.bat, change the second line to start:

  start jre/bin/javaw -Dhttp.proxyHost=proxyname.or.ip.address -Dhttp.proxyPort=proxy_port_number

Now, I get a list of CPUs and devices and it'll go off to download the data for the selected device.

0 项奖励
回复

6,048 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Stanislaw Klinke,

please what do you use for the Operating System?

Can you attach the screenshot of the error?

I´m including you the video, what I am able to see on my side.

Thank you for your feedback!

Best Regards,

Iva

0 项奖励
回复

6,048 次查看
stank
Contributor I

Hi Iva,

I am using Windows 7, 64-bit.

Below the screenshot of the issue. Problem is simple, I cannot select an MCU - the list is empty.

Capture.JPG

Kind Regards,

Stan

0 项奖励
回复

6,048 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Stanislaw,

I tested on 3 computers, Win7, 64-bit with the same successful result.

Please, did you try uninstall and install again? Did you have any problems during the installation?

Did you download it from here Kinetis Power Estimation Tool|Freescale ?

Thank you for your feedback!

Best Regards,

Iva

0 项奖励
回复

6,048 次查看
neilhancock
Contributor IV

It worked for me on a Win8.1

I was wondering what the schedule is of supporting processors Kinetis K

pastedImage_0.png

Processor support seems  good coverage on the Kinetis L and limited on the K - though appreciate its  V1.0 :smileyhappy:  

I'm particularly interested in MK26FN 

Playing with, I really like it is a visual manual for the processors - for instance on the MK22FN

playing with the  LPUART0 and UART0 for different baud rates is really valuable.

I have implemented a MK26FN and put into VLPS where it drops to 170uA - but includes the UART4 - so gives me some other ideas of what peripherals to play with. Looks a nice tool.

0 项奖励
回复

6,048 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Neil,

thank you for your feedback.

At the moment we cannot share such information about supported devices in future for this tool.

I will let you know in case of some changes.

Have a great day!

Iva

0 项奖励
回复