Config Tools 4.0 & MKL16Z128VFT4drivers issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tools 4.0 & MKL16Z128VFT4drivers issue

1,626 Views
palvepalamalych
Contributor I

Hello. I am new to this tool.

I made a configuration for the MKL16Z128xxx4 in MCUXpresso.

And get this warning:

Warning: Unsupported version of the SPI Driver in the toolchain/IDE project. Required: 2.0.4, actual: 2.0.3.

pastedImage_1.png

How can i solve this problem? 

0 Kudos
Reply
1 Reply

1,395 Views
marek-trmac
NXP Employee
NXP Employee

Hi Palve.

The warning is displayed because there is driver in the project, that was not tested with Peripherals.

Go to http://mcuxpresso.nxp.com and download latest version of the SDK package. Peripherals tool was tested with SDK 2.3.0.

It might work also with previous SDK version, but it was not tested.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button