i used kineties bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i used kineties bootloader

4,502件の閲覧回数
sreeramadhanala
Contributor I

I  used kineties bootloader with KL25Z.

it shows following error,

 

Error: Connect device failed(Error: Initial ping failure: No response received for ping command.).

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

4,126件の閲覧回数
harshpatel
Contributor IV

Hello Sreerama Dhanalakshmi

Fan_Yang is right. Check your UART communication first if you are using your custom hardware.

Connect your hardware to PC (you can use putty or access port etc) and send 0x5A 0xA6 and check is there any output given by hardware while running bootloader?

Bootloader code will acknowledge  0x5A 0xA6 command.   

Let me know if any..

Regards,

Harsh

0 件の賞賛
返信

4,126件の閲覧回数
ramboyang
NXP Employee
NXP Employee

Hi

Which board are you using? FRDM-KL25/TWR-KL25 or customized development board?

If you are using the NXP designed board, there should be no such issue.

If you are using a customized board, please ensure that the default PINMUX in the bootloader code matches your board design.

0 件の賞賛
返信

4,126件の閲覧回数
ramboyang
NXP Employee
NXP Employee

Hi,

Please provide detailed information like below, so that we can try to find out the root cause together and figure out the solution.

1. Kinetis Bootloader version

2. Peripheral

3. Speed

Thanks

Fan

0 件の賞賛
返信

4,126件の閲覧回数
sreeramadhanala
Contributor I

Hi,

Thank u for ur Reply.

1.I used Kinetis Bootloader version 2.0.0

2.KL25Z128VLK4

3.48Mhz speed

Thank u

0 件の賞賛
返信

4,126件の閲覧回数
ramboyang
NXP Employee
NXP Employee

Hi,

Regarding the Peripheral, I mean UART/SPI/I2C/USB HID, please let us know which peripheral you are talking to now:)

0 件の賞賛
返信

4,126件の閲覧回数
sreeramadhanala
Contributor I

Thank u for ur Reply,

I used UART ,By using Kineties Flash loader, it shows Following ERROR

Error: Connect device failed(Error: Initial ping failure: No response received for ping command.).

1.KL25Z128VLK4

2.Kinetis Bootloader version 2.0.0

3.UART communication

Thank u  .

0 件の賞賛
返信