Tool for pre-flashing LPC546

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tool for pre-flashing LPC546

4,714件の閲覧回数
jana_beck
Contributor II

Hello,

is there any device I can buy for flashing an MCU (LPC54606J512BD) before it gets soldered onto a PCB?
I am trying to save one step on the production line.

Thank you!

Jana

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

4,636件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Elnec have device programmers that include support for LPC546xx devices. They might have something for you: https://www.elnec.com/en/search/

 

0 件の賞賛
返信

4,646件の閲覧回数
jana_beck
Contributor II

Hi Rong,
thank you for your answer.

I was hoping to find an off-the-shelf solution, but sounds like I have to design it myself.

So in total I would need:
- socket (to plug in the MCU)
- pull up resistors (puts MCU in ISP mode)
- connector for connecting an external flashing tool (like Flash Magic)
- I also need to power the MCU right?

Thank you,
Jana

0 件の賞賛
返信

4,646件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jana,

Yes, there is not the  off-the-shelf solution, you have to develop the board yourself. On the board, the socket, pull-up/down resistors for the ISP pins, connector, power supply are required.

BR

XiangJun Rong

0 件の賞賛
返信

4,646件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jana,

For production flash programming before it gets soldered onto a PCB, I suppose that you can develop a target board which integrates a socket which adapts to your package of LPC54606J512BD. After the flash is written, you can pop up the processor from the socket.

You can use the blhost tools or Flash magic tools to download code, in the condition, the processor must be in ISP mode.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信