Serial Downloader mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial Downloader mode

3,217 Views
GaganaTN
Contributor I

Hi all,

 
We have designed a board using the i.MXRT1050 evk board scheme, but nothing changed. We are unable to detect the board in serial boot mode.
Tried the same thing with the Evaluation board and its working fine checked with all the schemes compared with our manufactured board and evaluation board, but couldn't find any solution, and we are stuck at the final stage of our project. It would be of great help if there is any solution  for this you can provide.
 
Thanks & Regards,
Gagana
0 Kudos
Reply
3 Replies

3,190 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

What is the state of the boot_mode pins? What process are you following to enter serial download mode?

Best regards,
Omar

0 Kudos
Reply

3,178 Views
GaganaTN
Contributor I

Hi @Omar_Anguiano ,

BOOT_MODE[1:0] (SW7-3 SW7-4)

01
Serial Downloader

This is the configuration done on 3rd and 4th switch in sw7 for serial downloader mode.

Thanks & Regards,

Gagana

0 Kudos
Reply

3,157 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

First, the ROM code polls the UART1 signals from TXD1/RXD1. Add a 10-kΩ pull up resistor to the TXD1/RXD1 pins to avoid an invalid trigger of the UART port in serial download.

Best regards,
Omar

0 Kudos
Reply