Flash download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash download

1,348件の閲覧回数
814420552
Contributor III

pastedImage_1.png

Hello, I got a problem when I  used ULINK to download code to flash, Can you give me some help? 

pastedImage_1.png

and when i connect Freemaster it has one problem as the above screenshot, wish for your help!

0 件の賞賛
返信
1 返信

1,258件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi kui wu,

   What the board you are using? The official board or your own designed board?

   If it is your own designed board, do you make it works in the previous time?

  Please also let me know your chip part number, when you download the code, the code also should related to your chip.

  If you have the JLINK, you can use the JLINK commander to check your board, can you find the ARM core or not?


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信