Flash download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash download

1,345 Views
814420552
Contributor III

pastedImage_1.png

Hello, I got a problem when I  used ULINK to download code to flash, Can you give me some help? 

pastedImage_1.png

and when i connect Freemaster it has one problem as the above screenshot, wish for your help!

0 Kudos
Reply
1 Reply

1,255 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi kui wu,

   What the board you are using? The official board or your own designed board?

   If it is your own designed board, do you make it works in the previous time?

  Please also let me know your chip part number, when you download the code, the code also should related to your chip.

  If you have the JLINK, you can use the JLINK commander to check your board, can you find the ARM core or not?


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply