SMC(Secure Monitor Call) for SMP on NXP S32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMC(Secure Monitor Call) for SMP on NXP S32V234

2,434 Views
tom_yeon
Contributor I

Hi, This is tom.

I'm porting vxWorks BSP on top of NXP S32V234.

I tried to call SMC to wake the secondary CPUs, but the system reboots right after calling SMC.

See the log1 for u-boot information.

1. I wonder the boot code supports SMC standard.

2. Is there any other way to wake the secondary CPUs for S32V234?

thanks

tom.yeon

log1)

U-Boot 2016.01+gf97fe2b7d3 (Apr 11 2018 - 18:48:58 +0200)

CPU:   NXP S32V234 V2.0 at 1000 MHz
Reset cause: unknown reset
Board: mpxs32v234-R2
I2C:   ready
DRAM:  2 GiB
RTC:   PCF85263
All (4) cores are up.
MMC:   FSL_SDHC: 0

Labels (1)
0 Kudos
Reply
1 Reply

2,257 Views
paulvlase
NXP Employee
NXP Employee

Hi [email protected]‌,

Right know we support only the Vision SDK in NXP Model-Based Design Toolbox for Vision and we don't have enough expertise on hardware related problems.

We recommend you to ask about this error in S32 Design Studio‌ community, they should know more about the S32V234 hardware.

0 Kudos
Reply