Getting started guide for S32R27

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started guide for S32R27

2,579件の閲覧回数
chidvilas_y
Contributor II

Hi,

I'm using S32 design studio with SW32R274_RSDK_RTM_1_0_0. I'm able to import projects and run them.

But I'm unable to get "printf" working.

I've even tried enabling the macros "UART_ENABLED" or "PE_SEMIHOSTING_EN"  from the Makefile. With UART_ENABLED macro it is throwing an error at #include "uart.h" and with PE_SEMIHOSTING_EN the error is thrown at linking and __read_console, __write_console etc are not found.

Is there any getting started guide to S32R27 debugging?

Can you give me the link to example UART application code that runs on this board?

Thanks,
Chidvilas

0 件の賞賛
返信
1 返信

2,392件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Here on the Model-Based Design community we handle questions regarding our toolboxes or other MATLAB/Simulink related question. You can find support for your question on the S32DS community (here). I did a little search and found this topic that might help you. Maybe you can test your options against the test example provided in that thread and compare them. Just a thought.

Hope this helps,

Razvan.

0 件の賞賛
返信