Question on freeMASTER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question on freeMASTER

5,596 次查看
vpandey1
Contributor I

Hi there

I'm new to using freeMASTER & would appreciate if someone can help with following

1. How to use a command line to issue START command to freeMASTER to start with logging. For our test application running NI labview, command needs to be issued to freeMASTER to start the data logging. The unit under test is connected to PC through USB port and at power up embedded code will start with internal checks on unit & start outputting messages on USB com port. The power up is done using labview code.

2. Once data is logged need to save logged data to excel file. Please help on how to save data to excel file.

Thanks

Vinod

标记 (1)
0 项奖励
回复
2 回复数

2,650 次查看
kadanik
Contributor II
0 项奖励
回复

5,545 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

I think for your question you will find a proper answer on the FreeMASTER community space.

Hope this helps,

Marius

0 项奖励
回复