1. Adaptive Dynamic Headlights with Pedestrian Spotlight Function - by eVision Team members: Balaban Valeriu - Master, Advanced Microelectronics, Electronics, UPB Voicu Tudor Alexandru - Bachelor, Applied Electronics, Electronics, UPB Stanescu Sebastian - Bachelor, Telecom Networking and Software, UPB Short description: Because of the high rate of fatalities between night accidents a lot of research are held for developing techniques to increase the driver area of vision during the night and to reduce the accident damage if this could not be avoided. The adaptive headlight function helps to see further in poor light conditions and especially in bends: the cornering light swivels the headlights in the direction of travel, with the degree of turn computed by a CPU, to illuminate as much road area as possible An interesting solution is spotlight lighting function, which is a LED beam that specifically illuminates potential hazards. If the near infrared camera detects deer at the roadside or pedestrians on the road, they can be briefly illuminated beyond the normal area covered by the main beams, by a spot-light to attention the driver for a possible danger. Presentation: Please consult eVisionPresentation.pdf. Documentation: Please consult eVisionDoc.pdf. Code Sources https://github.com/izzi/app-evision https://github.com/izzi/meta-evision 2. Voice Commanded Interface for DriverVehicle Interaction - by She# Team members: Iulia Neagoe - Computer Sciences and Military Information Systems,Military Technical Academy Mihaela-Anca Sorostinean - Computer Sciences and Military Information Systems,Military Technical Academy Short description: In the context of continuous technological advances in the automotive and communications domains, a drivers responsibility has switched from just controlling the car to interacting with the multitude of gadgets provided by the manufacturer. The purpose of this project is to design an interface that offers the driver the possibility of controlling some of the nonvital functionalities of the car by vocal commands, so as to enable the driver to focus his attention on the road while also having a comfortable mean of communication with the car. We developed a system of vocal recognition of some basic features like the radio, windows, clima or a phone which we implemented on the Wandboard. Also we provide the user with a graphical interface of the recognized commands in order to enhance his interaction with the vehicle. Presentation: Please consult ShePresentation.pdf. Documentation: Please consult SheDoc.pdf. Code Sources Please see She#_Project_Source.zip. 3. Driving Control Software - by FreeSoftwares Team members: Petrosanu Adrian-Sabin - Computer Science, UPB Birsan Nicoleta Cosmina - Computer Science, UPB Radoi Ioana Gabriela - Computer Science, UPB Short description: "Driving Control Software" is a soft to control an automatic gearbox. This project consists of simulating the behavior of an automatic gearbox on the Wandboard. An automatic gearbox is a type of motor vehicle transmission that can automatically change gear ratios as the vehicle moves. Presentation: Please consult FreeSoftwaresPresentation.pdf. Documentation: Please consult FreeSoftwaresDoc.pdf. Code Sources Please see Freesoftwares_Project_Source.zip. 4. Autonomous Car Parking - by ATM Team members: Mihai Coca - Computer Sciences and Military Information Systems,Military Technical Academy Georgian Andrei - Computer Sciences and Military Information Systems,Military Technical Academy Hiji Iulian - Computer Sciences and Military Information Systems,Military Technical Academy Short description: A large number of companies are developing autonomous vehicle technology through applying its work in the area to a particular usage case : parking. The purpose of this project is to design a concept vehicle, which can be dropped off at the curb by its owner and left to its own devices to enter into a spot park. The process can even be reversed when the owner is ready to go, with the car leaving the spot park on its own to meet its key-holder again at the curb. Documentation: Please consult ATMDoc.pdf Code Sources Please see ATM_Project_Source.zip. 5. Collision Detection - by Beer2.0 Team members: Nitu Adrian - Computer Science, UPB Short description: The purpose of our project is to provide cars with a sense of the road ahead and enable it to take preventive actions against collisions; In this way we hope to reduce accidents on the road. It will gather signals and informations from different hardware and will alert the driver or take immediate control of the car in order to make critical maneuvers in order to protect the driver from any life threatening event. A Freescale Cup car will be equipped with a Wandboard and two USB cameras so we can track the environment. After initial object tracking we will incorporate Human Interaction by remote control. For this project we believe a simple warning system and/or breaking will suffice as a proof of concept. Presentation: Please consult Beer20Presentation.pdf Documentation: Please consult Beer20Doc.pdf Code Sources https://bitbucket.org/adriannitu92/freechallenge 6. Feedforward adaptive noise cancellation using sub-band normalized filtered-X LMS algorithm - by Brainiacs Team members: Cristian Monea - Telecommunications and Information Technology, Electronics, UPB Madalin Zaharia - Telecommunications and Information Technology, Electronics, UPB Short description This project proposes a feedforward adaptive noise cancellation (ANC) algorithm based on sub-band normalized filtered-X LMS (NFXLMS). The use of an adaptive algorithm offers advantages over simple filtering algorithms like fixed FIR or IIR filters. Also, noise generated in a car environment can be considered stationary because it preserves some of its properties, like spectral distribution, mean, variance, which allows the use of adaptive filters in car noise cancellation applications. The feedforward system should be more efficient than feedback systems. In this case, a coherent reference noise input is sensed before it propagates past the canceling speaker. Thus, the algorithm will simulate the two sensors (microphones): reference sensor, which measures the primary noise to be canceled, and the error sensor. Presentation: Please consult BrainiacsPresentation.pdf Documentation: Please consult BrainiacsDoc.pdf
記事全体を表示