using LX2160A-RDB Reference Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using LX2160A-RDB Reference Board

2,572 Views
16624486
Contributor I

If using LX2160A-RDB Reference Board, should we need to connect codeWarrrior@TAP to the LX2160A-RDB for system debug ? 

Tags (1)
0 Kudos
Reply
3 Replies

2,457 Views
16624486
Contributor I

I mean, how to use the LX2160A-RDB reference board?

Should we need to use the simulator(code Warrior@TAP) to connect the computer to  LX2160-RDB to evaluate LX2160A?

or just need the other cable to connect the computer to LX2160-RDB? 

0 Kudos
Reply

2,457 Views
ufedor
NXP Employee
NXP Employee

The board is provided fully operational, with latest NXP LSDK firmware installed.

The DB9 shielded serial cable (to connect console to the host PC) is included in the RDB kit.

Pre-built firmware images can be programmed by means of U-Boot using Ethernet (Cat-6 Ethernet cable is included) TFTP to transfer them from host PC.

Of course the CodeWarrior IDE, CodeWarrior TAP and Probe Tip are required for software debugging.

0 Kudos
Reply

2,457 Views
ufedor
NXP Employee
NXP Employee

Sorry, the request is not fully clear - please elaborate.

0 Kudos
Reply