rte_eth_rx_burst -> returning same mbuff pointer twice consecutively

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rte_eth_rx_burst -> returning same mbuff pointer twice consecutively

978 Views
Chidananda22
Contributor IV

From my application calling rte_eth_rx_burst 

checking sometimes same mbuff coming twice . Checked code buffer not freeing . With out mbuff free what could be the scenario that same mbuff pointer received twice .

Labels (1)
0 Kudos
Reply
5 Replies

971 Views
yipingwang
NXP TechSupport
NXP TechSupport

Without an explicit mbuf free in your code, the most likely scenarios are that the mbuf is still being effectively returned/reused through another path in the application or shared unsafely across threads/cores, or that a special driver/path-specific buffer handling issue is corrupting lifecycle state.

  • Cross-core/shared mbuf ownership issue. One documented case used one CPU for RX and many worker CPUs consuming mbufs from a ring; the mbuf address was then seen reused/overwritten while still referenced elsewhere. NXP specifically asked whether RTE_MBUF_REFCNT_ATOMIC was enabled for multicore access, and the customer said yes, but the issue was still treated as application-level ownership/lifetime handling.,
  • Duplicate release or hidden return path in the application pipeline. NXP’s guidance in that case was to instrument buffer allocate/release/packet-send actions to see whether the same address was being released back to the buffer pool more than once.
  • PMD/driver returning malformed mbufs to pool in special paths. There is a separate DPAA2 PMD case involving chained mbufs where mbufs returned to the mempool appeared corrupted ( next not cleared), causing sanity-check failures on later allocation. That is not the same symptom as your report, but it does show that special buffer handling paths can lead to later reuse/corruption symptoms.
  • Same source and destination mbuf in crypto path. In a DPAA security/IPsec case, NXP noted that if sym->m_dst is NULL , then m_src and m_dst use the same mbuf. That can make packet contents appear rewritten “in place” under load, even though the pointer identity did not change.

 

0 Kudos
Reply

962 Views
Chidananda22
Contributor IV

thanks @yipingwang  for your quick reply and suggestions. from code i am not to figure out more . Any DPDK debug flag can help ? 

0 Kudos
Reply

936 Views
yipingwang
NXP TechSupport
NXP TechSupport
  1. Enable DPDK log levels (first thing to try)

Run your app with:

--log-level=8

What you’ll see:

  • RX descriptor handling
  • buffer allocation/recycling
  • PMD behavior
  1. Enable mbuf debug checking (very useful)

Rebuild DPDK with:

CONFIG_RTE_LIBRTE_MBUF_DEBUG=y

This will:

  • Validate mbuf consistency
  • Catch:
    • corrupted metadata
    • reused mbuf incorrectly
    • invalid refcnt

 

  1. Enable mempool debug

      CONFIG_RTE_LIBRTE_MEMPOOL_DEBUG=y

Helps detect:

  • double allocation
  • cache corruption
  • same buffer returned twice from mempool

 

  1. Poison/free tracking (EXTREMELY useful)

You can enable memory overwrite checking:

CONFIG_RTE_MALLOC_DEBUG=y

and

--mp-alloc=debug

This helps detect:

  • overwrite before/after mbuf
  • hidden memory corruption

 

  1. Quick isolation trick (VERY effective)

Run

testpmd -- -i

Then:

set fwd rxonly

start

 

If duplication disappears:

  • your application bug

If still happens:

  • PMD / HW / queue config issue
0 Kudos
Reply

926 Views
Chidananda22
Contributor IV

Thanks @yipingwang  for Quick reply . I will try and update you .

One observation every time multiple mbuf ( same address coming ) getting below prints in screen

 

fslmc: dpaa2_get_qbman_swp(): New Portal 0x17ffd61c0 (5) affined thread - 1953
fslmc: dpaa2_configure_stashing(): Portal= 5 CPU= 10 SDEST= 5
fslmc: DPAA Portal=0x17ffd61c0 (5) is affined to thread 1953

0 Kudos
Reply

870 Views
yipingwang
NXP TechSupport
NXP TechSupport
Those fslmc / dpaa2 portal affined thread logs strongly indicate portal (QBMan SWP) is being re-attached to a different thread/core, which can break ownership model → leading to mbuf reuse / duplication symptoms.
0 Kudos
Reply