restool create dpmac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

restool create dpmac

4,792 Views
dsouthwi
Contributor III

Hello,

I'm looking for info/help on how restool/MC-utils determines the number of dpmac devices that are available, and how I can modify this. Does it have it's own SERDES lookup table somewhere?

For example on the lx2160a:

If I boot with SD1=8, I see 8 dpmac devices corresponding the 8xUSXGMII lanes.

If I boot with SD1=17, I see 4 dpmac corresponding the the 4x25GE (and none for PCIe lanes).

If I boot with SD1=17 (modified to have 4x25G+4xUSGMII) I only get 4 dpmac.

Modifying the DPL file to declare more dpmac lanes is discarded/ignored by restool.

Modifying the SERDES definition in u-boot SERDES table is discarded/ignored by restool.

Trying to manually add more dpmac via restool results in :

> restool dpmac create --mac-id=7  #create dpmac.7
MC error: Invalid state (status 0xc)
> restool --mc-version
MC firmware version 10.28.1

My SFP modules are detected during kernel boot in the USXGMII lanes, but I cannot create dpni objects as I lack dpmac for them. I can use the 25G dpmac however.

I have modified my SERDES (following Application Note #AN13022) to have 4x25G+4xUSXGMII, but I cannot determine what in LSDK21.08 is blocking MC-utils from creating dpmac for these interfaces.

Is there any documentation / help on this?

Labels (1)
0 Kudos
Reply
5 Replies

4,783 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "26.1.4 SerDes options" in LX2160ARM.pdf, dpmac number is determined by SerDes 1 protocol(RCW[SRDS_PRTCL_S1]), you cannot add more dpmac lanes.

0 Kudos
Reply

4,776 Views
dsouthwi
Contributor III
Right, I understand what the reference manual says, but I am referring to https://www.nxp.com/docs/en/application-note/AN13022.pdf where they state "MC firmware versions 10.24.1 and later add support for [serdes] protocol 31". Where is the information related to MC and protocol 31 limitation, etc?
0 Kudos
Reply

4,751 Views
yipingwang
NXP TechSupport
NXP TechSupport

If configuring SerDes 1 as protocol 31, you only can get 4xUSXGMII lanes, you only can get 4 DPMACs for these interfaces. It is still impossible to add more dpmacs manually.

0 Kudos
Reply

4,398 Views
dsouthwi
Contributor III

Given that recent DPAA2 MC firmware support changing the DPMAC lane speeds (see DPAA2 user manual for 10.36.x, section 15.2.21 DPMAC_SET_PROTOCOL ) would it be possible to change the protocol from 25G to 10G?

0 Kudos
Reply

4,690 Views
dsouthwi
Contributor III

Hmm. I have been provided with a validated pbi override that performs the above for SERDES, but it seems I need a new (different) behavior for the MC complex, as I understand from you that 31 is a fixed profile that does not match my needs. It's unfortunate that the MC does not read the serdes configuration directly, and instead operates off it's own table, making it the point of failure in this scenario.

0 Kudos
Reply