random: udevd: uninitialized urandom read (16 bytes read)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

random: udevd: uninitialized urandom read (16 bytes read)

2,289件の閲覧回数
ThomasMeyer
Contributor I

Hi Community,

at the end of the boot sequence from my own image I´ve got the following messages ( warnings?)

[ 2.813429] Run /sbin/init as init process
[ 2.833386] random: fast init done
INIT: version 2.97 booting
Starting udev
[ 3.632096] udevd[99]: starting version 3.2.9
[ 3.654688] random: udevd: uninitialized urandom read (16 bytes read)
[ 3.663675] random: udevd: uninitialized urandom read (16 bytes read)
[ 3.670378] random: udevd: uninitialized urandom read (16 bytes read)
[ 3.728846] udevd[100]: starting eudev-3.2.9
[ 4.520745] EXT4-fs (mmcblk0p4): re-mounted. Opts: (null)
[ 5.018291] urandom_read: 4 callbacks suppressed
[ 5.018304] random: dd: uninitialized urandom read (512 bytes read)
INIT: Entering runlevel: 5

Anyone have an idea what that could mean?And how to fix it ?

Looks to me like the bootsequence isn't right? 

Thanks in advance

0 件の賞賛
返信
0 返答(返信)