Hello,
I am trying to synchronize some NXP equipment using ptp4l. It works fine for all the other boards, but I am facing a problem with the LS1028ARDB.
I run the following command :
# ptp4l -i swp0 -i swp1 -f /etc/ptp4l_cfg/gPTP.cfg
But it returns this error (besides the fact that the offsets remain very high):
ptp4l[xxxx.xxx]: clockcheck: clock jumped backward or running slower than expected!
Can you help me to identify what is the problem there?
Thank you.
cerrone
You will find the gPTP .cfg file attached below.
Solved! Go to Solution.
Could you try adding 'step_threshold 0.00002' setting to the gPTP.cfg file pls and let us know whether the situation is improved ?
(for more info ref: https://github.com/openil/linuxptp/issues/10)
> So could this phc_ctl command be the cause of the problem ?
It seems that a large change in PHC is difficult to tune for, so these gPTP.cfg tunings should help.
In fact it was allready commented, I forgot to indicate it in my previous message.
Another thing that I forgot to say: before lauching ptp4l on each board, I also reset the PTP Hardware Clock. On the LS1028ARDB, the exact command that I run is:
# phc_ctl /dev/ptp1 set 0; ptp4l -i swp0 -i swp1 -f /etc/ptp4l_cfg/gPTP.cfg -m
(I reset the PHC on every board, but the LS1028ARDB is the only one on which I get the error message...)
So could this phc_ctl command be the cause of the problem?
ceroone
Could you try adding 'step_threshold 0.00002' setting to the gPTP.cfg file pls and let us know whether the situation is improved ?
(for more info ref: https://github.com/openil/linuxptp/issues/10)
> So could this phc_ctl command be the cause of the problem ?
It seems that a large change in PHC is difficult to tune for, so these gPTP.cfg tunings should help.
my test step is :
1、start the master run ptp4l and phc2sys
2、start the slave device , run ptp4l and phc2sys
then slave system clock is sync sucsess by master., all this step is run ok。
then i use date 081515302023 to change master's time ,the time chagne maybe 1 minutes or more larger, maybe 1 hour or one day.
then the slave device print error message:
clockcheck: clock jumped forward or running faster than expected!
So my question is ;
1、the ptp can't chagne master's time too large, It do not suporrt? My test method is wrong 。
(I do this is want to confirm: the slave's time can change with the slave's time)
or
2、the cmd I use i not corret, or the confiuge is not correct? I use date cmd to change master's time
so large is ok, there is no problem?
can you help me anser my question ,thank you !
Adding "step_threshold 0.00002" seems to solve the problem indeed.
Thank you !
Hi:
my slave device use cmd :
my test step is :
1、start the master run ptp4l and phc2sys
2、start the slave device , run ptp4l and phc2sys
then slave system clock is sync sucsess by master., all this step is run ok。
then i use date 081515302023 to change master's time ,the time chagne maybe 1 minutes or more larger, maybe 1 hour or one day.
then the slave device print error message:
clockcheck: clock jumped forward or running faster than expected!
So my question is ;
1、the ptp can't chagne master's time too large, It do not suporrt? My test method is wrong 。
(I do this is want to confirm: the slave's time can change with the slave's time)
or
2、the cmd I use i not corret, or the confiuge is not correct? I use date cmd to change master's time
so large is ok, there is no problem?
can you help me anser my question ,thank you !
In gPTP.cfg, please comment out the neighborPropDelayThresh line
# neighborPropDelayThresh 800
and let us know how you get on.