network interface not working properly in ls1028a with specific serdes configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

network interface not working properly in ls1028a with specific serdes configuration

3,147 Views
Hamza
Contributor II

Hi,

We are currently using the layerscape module ls1028a in our custom board these are the network configuration that we are interested to use in our project.

SRDS_PRTCL_S1 = 0x9999

Hamza_0-1697537193086.png

 

 

Reset Configuration Word (RCW):
       00000000: 34004010 00000030 00000000 00000000
       00000010: 00000000 008e0000 0030c000 00000000
       00000020: 01403150 00002580 00000000 000080de
       00000030: 00000000 00000010 00000000 00000000
       00000040: 00000000 00000000 00000000 00000000
       00000050: 00000000 00000000 00000000 00000000
       00000060: 00000000 00000000 000e7000 00000000
       00000070: 99990000 03000000
Using SERDES1 Protocol: 39321 (0x9999)

 

 

Device tree:

 

 

&enetc_port0 {
status = "disabled";
};

&enetc_port1 {
status = "disabled";
};

&enetc_mdio_pf3 {
mdio1_sgmii_phy01: ethernet-phy@1 {
reg = <0x01>;
};
};

/* l2switch ports */
mxl8153_port0: &mscc_felix_port0 {
status = "okay";
phy-mode = "sgmii";
fixed-link {
speed = <1000>;
full-duplex;
};
};

rj45_port1: &mscc_felix_port1{
status = "okay";
phy-mode = "sgmii";
phy-handle = <&mdio1_sgmii_phy01>;
};

sfp_port3: &mscc_felix_port2 {
status = "okay";
phy-mode = "1000base-x";
sfp = <&sfp_neta>;
fixed-link {
speed = <1000>;
full-duplex;
};
};

&mscc_felix_port3{
status = "disabled";
phy-mode = "sgmii";
};
~# ip a
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host
       valid_lft forever preferred_lft forever
2: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000
    link/sit 0.0.0.0 brd 0.0.0.0
3: eno2: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1520 qdisc mq state UP group default qlen 1000
    link/ether 00:d0:93:5a:58:89 brd ff:ff:ff:ff:ff:ff
    altname enp0s0f2
    inet6 fe80::2d0:93ff:fe5a:5889/64 scope link
       valid_lft forever preferred_lft forever
4: swp0@eno2: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue state UP group default qlen 1000
    link/ether 00:d0:93:5a:58:89 brd ff:ff:ff:ff:ff:ff
    inet 192.168.1.99/24 brd 192.168.1.255 scope global swp0
       valid_lft forever preferred_lft forever
    inet6 fe80::2d0:93ff:fe5a:5889/64 scope link
       valid_lft forever preferred_lft forever
5: swp1@eno2: <BROADCAST,MULTIpiCAST,UP,LOWER_UP> mtu 1500 qdisc noqueue state UP group default qlen 1000
    link/ether 00:d0:93:5a:58:89 brd ff:ff:ff:ff:ff:ff
    inet 192.168.3.99/24 brd 192.168.3.255 scope global swp1
       valid_lft forever preferred_lft forever
    inet6 fe80::2d0:93ff:fe5a:5889/64 scope link
       valid_lft forever preferred_lft forever
6: swp2@eno2: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc noqueue state UP group default qlen 1000
    link/ether 00:d0:93:5a:58:89 brd ff:ff:ff:ff:ff:ff
    inet 192.168.2.99/24 brd 192.168.2.255 scope global swp2
       valid_lft forever preferred_lft forever
    inet6 fe80::2d0:93ff:fe5a:5889/64 scope link
       valid_lft forever preferred_lft forever
~# dmesg | grep felix
[    2.878838] mscc_felix 0000:00:00.5: Adding to iommu group 0
[    3.938295] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[    3.945147] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[    3.951985] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[    3.982181] mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[    3.989402] mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control rx/tx
[    4.016168] mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:01] driver [RTL8211F Gigabit Ethernet] (irq=POLL)
[    4.028004] mscc_felix 0000:00:00.5 swp2 (uninitialized): switched to inband/1000base-x link mode
[    7.462744] mscc_felix 0000:00:00.5 swp0: configuring for fixed/sgmii link mode
[    7.482654] mscc_felix 0000:00:00.5 swp0: Link is Up - 1Gbps/Full - flow control off
[    7.531142] mscc_felix 0000:00:00.5 swp1: configuring for phy/sgmii link mode
[    7.586585] mscc_felix 0000:00:00.5 swp2: configuring for inband/1000base-x link mode
[    7.663844] mscc_felix 0000:00:00.5 swp2: Link is Up - 1Gbps/Full - flow control rx/tx
[   10.629362] mscc_felix 0000:00:00.5 swp1: Link is Up - 1Gbps/Full - flow control rx/tx
~# dmesg | grep enetc
[    0.788902] pci 0000:00:00.0: enetc_fixup_clear_rss_rfs+0x0/0x5c took 105157 usecs
[    0.896919] pci 0000:00:00.1: enetc_fixup_clear_rss_rfs+0x0/0x5c took 105457 usecs
[    1.004395] pci 0000:00:00.6: enetc_fixup_clear_rss_rfs+0x0/0x5c took 104925 usecs
[    2.885141] fsl_enetc 0000:00:00.2: Adding to iommu group 1
[    2.891055] fsl_enetc_mdio 0000:00:00.3: Adding to iommu group 2
[    3.004108] fsl_enetc_mdio 0000:00:00.3: enabling device (0400 -> 0402)
[    3.014087] fsl_enetc_ptp 0000:00:00.4: Adding to iommu group 3
[    3.020113] fsl_enetc_ptp 0000:00:00.4: enabling device (0404 -> 0406)
[    3.544114] fsl_enetc 0000:00:00.2: enabling device (0400 -> 0402)
[    4.037412] fsl_enetc 0000:00:00.2 eth0: entered promiscuous mode
[    7.215724] fsl_enetc 0000:00:00.2 eno2: renamed from eth0
[    7.427418] fsl_enetc 0000:00:00.2 eno2: configuring for fixed/internal link mode
[    7.442037] fsl_enetc 0000:00:00.2 eno2: Link is Up - 1Gbps/Full - flow control rx/tx
~# ethtool swp1
Settings for swp1:
        Supported ports: [ TP    MII ]
        Supported link modes:   10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Full
        Supported pause frame use: Symmetric Receive-only
        Supports auto-negotiation: Yes
        Supported FEC modes: Not reported
        Advertised link modes:  10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Full
        Advertised pause frame use: Symmetric Receive-only
        Advertised auto-negotiation: Yes
        Advertised FEC modes: Not reported
        Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                             100baseT/Half 100baseT/Full
                                             1000baseT/Full
        Link partner advertised pause frame use: Symmetric Receive-only
        Link partner advertised auto-negotiation: Yes
        Link partner advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Auto-negotiation: on
        master-slave cfg: preferred slave
        master-slave status: slave
        Port: Twisted Pair
        PHYAD: 1
        Transceiver: external
        MDI-X: Unknown
        Supports Wake-on: d
        Wake-on: d
        Link detected: yes

 

 

The problem that I’m facing is that I’m not able to ping (send/receive data) using the interface swp1 (RJ45).

We tried to remove the flow control rx/tx using the ethtool using the following command before assigning an ip address to the interface and I was able to ping :

 

 

~# ethtool -A swp1 autoneg off rx off tx off
~# [ 128.775236] mscc_felix 0000:00:00.5 swp1: Link is Down
[ 131.557587] mscc_felix 0000:00:00.5 swp1: Link is Up - 1Gbps/Full - flow control off ping 192.168.3.222
PING 192.168.3.222 (192.168.3.222): 56 data bytes
64 bytes from 192.168.3.222: seq=0 ttl=128 time=0.861 ms
64 bytes from 192.168.3.222: seq=1 ttl=128 time=0.674 ms

 

 

Unfortunately, I lose the connection (ping) if I remove and replug the cable, if I try to test the interface from ethtool

 

 

~# ethtool -t swp1
The test result is FAIL
The test extra info:
 1. Carrier                      0
 2. PHY dev is present           0
 3. PHY internal loopback, enab  0
 4. PHY internal loopback, UDP   -110
 5. PHY internal loopback, MTU   -110
 6. PHY internal loopback, TCP   -110
 7. PHY internal loopback, disa  0 

 

 

 

This behavior is the same for linux kernel version 5.15 , 6.1.35 and 6.5.7 (we wanted to make sure that it was not a driver issue that is fixed in a newer version)

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

3,102 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello

" This behavior is the same for linux kernel version 5.15 , 6.1.35 and 6.5.7 (we wanted to make sure that it was not a driver issue that is fixed in a newer version) " - It isn't a driver issue, did you follow the steps in chapter 29.7.1.1 1G SGMII in the ls1028ARM? it looks like an issue related to the Auto-N.

0 Kudos
Reply

3,006 Views
Hamza
Contributor II

Hi @Oswalag 

I confirm that this is issue is related to auto negotiation in fact, the uboot driver is setting up everything correctly but the problem starts when booting to kernel.

affected registers
29.6.9.2 SGMII Control (SGMII_CR)
29.6.9.18 SGMII IF Mode (SGMII_IF_MODE)

before enabling the network interface both registers values are the same as the uboot initialization.

After enabling the network interface both registers values changes and the interface became unusable.

 ip link set dev <interface> up
or 
 ip link set dev <interface> down

when we restart the service systemd-networkd we lost the connection with the interface.

systemclt restart systemd-networkd

to restore the interface we need to launch these commands which basically reinitialize the values into the registers as described in (29.7.1.1 1G SGMII).

devmem2 0x1f8148034 w 0x34
devmem2 0x1f8148038 w 0x3
devmem2 0x1f8148034 w 0x20
devmem2 0x1f8148038 w 0x1200

 

Do you have any idea what is the reason behind this behavior ? if so, I would appreciate it if you can share some the solution to solve it.

Best regards,

0 Kudos
Reply

2,990 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please check the configuration of the registers,

This initialization says that there are 2 processes A and B. A is auto-negation process itself as discovering counterparts capabilities and B process as serdes PCS configuration for SGMII in accordance to the result of A process.

So when USE_SGMII_AN=0  the PCS operation should be programmed with the register bit SGMII_SPEED and SGMII_DUPLEX. When set to 1, the PCS operation is automatically programmed with the Partner abilities advertised during Auto-Negotiation.

0 Kudos
Reply