ls1046a linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046a linux

1,291 Views
renaud
Contributor IV

I got the ls1046a-rdb eval board running Linux 4.9.62. Is that the latest version to support the eval board?

 

I am trying to get Linux 5.11 to run. It start booting to the point where the kernel should acquire an IP address thru DHCP. It does not work. (the boot loader does acquire it so the server works).

Is the Ethernet support complete on Linux 5.11 as I can see much more code in 4.9.

Could you advise?

 

Cheers.

0 Kudos
Reply
1 Reply

1,280 Views
Pavel
NXP Employee
NXP Employee

NXP offers LSDK 2012 for the LS1046ARDB board:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap...

 

This LSDK supports LTS 4.19.139 and LTS 5.4.47 Linux kernel. See LSDK 2012 User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

 

Use this LSDK.

0 Kudos
Reply