ls1046a encryption tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1046a encryption tool?

1,647 次查看
aleksanderbiryu
Contributor I

Hello.

I want create encrypted linux image for ls1046a, then copy this image on flash.

Before booting, decrypt this image use "blob dec" u-boot command and then boot linux.

What tool can I use to create encrypted linux image on x86 host?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,497 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Aleksander Biryukov,

Please refer to the following Encap boot commands under u-boot.

nand read <uImage DDR> <uImage NAND> <uImage size>
esbc_blob_encap <uImage DDR> 0x10000000 <uImage size> 0x11223344556677889900aabbccddeeff
nand erase <encapsulated uImage NAND> <encapsulated uImage size>
nand write 0x10000000 <encapsulated uImage NAND> <encapsulated uImage size>

Please refer to the following decap boot commands under u-boot.

nand read <encapsulated uImage DDR> <encapsulated uImage NAND> <encapsulated uImage size>
esbc_blob_decap <encapsulated uImage DDR> 0x10000000 <uImage size>
0x11223344556677889900aabbccddeeff


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复