ls1046a DDR validation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046a DDR validation

883件の閲覧回数
renaud
Contributor IV

We are doing a design based on the LS1026. The DDR4 will be configured through SPD.

We do not have a Codewarrior ICE so I suppose I cannot run the DDR validation tool.

 

Is there an application note explaining the algorithm to use to tune up the DDR4?

I suspect the algorithm must loop on CLK_ADUST and WRLVL, run a BIST and see it is passes or not

I do have the QCVS_DDR user guide showing a validation tool.

 

0 件の賞賛
返信
1 返信

880件の閲覧回数
ufedor
NXP Employee
NXP Employee

You wrote:

> The DDR4 will be configured through SPD.

In this case, if DDR interface PCB layout will be implemented exactly as described in the AN5097 - Hardware and Layout Design Considerations for DDR4 SDRAM, then, normally, no additional optimization will be needed.

> Is there an application note explaining the algorithm to use to tune up the DDR4?

There is no such document.

0 件の賞賛
返信