ls1046 timestamp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ls1046 timestamp

1,441件の閲覧回数
kwangholee
Contributor I
Hi dear.
Does the ieee1588 timestamp function work on both Serdes1 Lane1 (SFP), Serdes 1 Lane0 (10g / 2.5g rj46), EC1 to EC4 on the LS1046?
0 件の賞賛
返信
1 返信

1,370件の閲覧回数
bpe
NXP Employee
NXP Employee


IEEE1588 timestamping unit is part of mEMAC which is behind SerDes or parallel
interface and works independently of the connection type or data rate.

Regards,

Platon

0 件の賞賛
返信