ls1046 timestamp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1046 timestamp

1,443 Views
kwangholee
Contributor I
Hi dear.
Does the ieee1588 timestamp function work on both Serdes1 Lane1 (SFP), Serdes 1 Lane0 (10g / 2.5g rj46), EC1 to EC4 on the LS1046?
0 Kudos
Reply
1 Reply

1,372 Views
bpe
NXP Employee
NXP Employee


IEEE1588 timestamping unit is part of mEMAC which is behind SerDes or parallel
interface and works independently of the connection type or data rate.

Regards,

Platon

0 Kudos
Reply