ls1028ardb rfs emmc fusing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1028ardb rfs emmc fusing

1,340 次查看
pjw
Contributor II

Hi 

I am using the ls1028ardb board.

succeeded in uploading kernel images using flex-build, tftp / code warrior.

Here's the question:
kernel img goes up to emmc, but rfs seem to go up to ram memory.
Because, when boot up the board, the files I created are reset.
So I want to put the RFS on emmc. If the root file system is uploaded to emmc, I think the file will not be erased.

I'm looking for related content in manual or flex-build guide, but it's hard to find.

I wonder if there is a similar content or a way to use flex-build or something. I want to know how to put the RFS on emmc using tftp or build boot.

Thank you!

0 项奖励
回复
1 回复

1,326 次查看
bpe
NXP Employee
NXP Employee

You must be booting your board with TinyLinux userland which is ramdisk based. It does not matter where it is fetched from, the changes you made are lost due to the used filesystem type. Consider deploying Ubuntu userspace with flex-installer. This rootfs image is ext2-based and preserves your changes.Details can be found at the links below:

 

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-63B176B2-CAC9-468B-9...

 

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-2C30B1D2-2E1A-49BC-A...

Hope this helps,
Platon

 

0 项奖励
回复