how to use flex-builder to making rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use flex-builder to making rootfs

ソリューションへジャンプ
6,148件の閲覧回数
muaxi8
Contributor V

lx2160ardb_rev2 platform;

How to generate a root file system using Flex-Builder

 

0 件の賞賛
返信
1 解決策
6,106件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
10 返答(返信)
6,144件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The default LSDK main userland is an Ubuntu 18.04 based hybrid userland with NXP's packages/components and system configurations. You can select the appropriate distro userland as per your need, the various userlands are showed in the table in page 182 of LSDK 20.12 user manual.

You could generate Ubuntu-based main userland with the following command.

$ flex-builder -i mkrfs -r ubuntu:main

$ flex-builder -i packrfs -r ubuntu:main

0 件の賞賛
返信
6,138件の閲覧回数
muaxi8
Contributor V

According to  "Unified 64MiB memory layout of NOR/QSPI/XSPI/NAND/SD media ", ramdisk isonly 32MB, but flex-builder maked the rootfs is 678862805 bytes,it is too big。

muaxi8_1-1627365469351.png

flex-builder -i packrfs -r ubuntu:main

muaxi8_0-1627365360094.png

 

0 件の賞賛
返信
6,134件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could use yocto-based tiny userland, it includes Yocto basic packages and
part of NXP's packages (restool, aiop_tool, tsntool, fmc, net-tools, flex-installer, ccsr,  etc).

$ flex-builder -i mkrfs -r yocto:tiny

 

Generates RAM-bootable FIT image, including Linux Kernel+ramdisk rootfs.

flex-builder -i mkitb -r yocto:tiny

0 件の賞賛
返信
6,129件の閲覧回数
muaxi8
Contributor V

 flex-builder -i mkrfs -r yocto:tiny

there are some errors, i can not get yocto-based tiny userland.

muaxi8_0-1627379293094.png

 

~/work/0734/flexbuild_lsdk2012$ flex-builder -i mkrfs -r yocto:tiny
INSTRUCTION: mkrfs
DISTRO TYPE: yocto
DISTRO SCALE: tiny

### Shell environment set up for builds. ###

You can now run 'bitbake <target>'

Common targets are:
core-image-minimal
core-image-sato
meta-toolchain
meta-ide-support

You can also run generated qemu images with a command like 'runqemu qemux86'

Other commonly useful commands are:
- 'devtool' and 'recipetool' handle common recipe tasks
- 'bitbake-layers' handles common layer tasks
- 'oe-pkgdata-util' handles common target package tasks
Loading cache: 100% |#######################################################################################################################################| Time: 0:00:00
Loaded 1305 entries from dependency cache.
Parsing recipes: 100% |#####################################################################################################################################| Time: 0:00:00
Parsing of 776 .bb files complete (772 cached, 4 parsed). 1305 targets, 59 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.44.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "qemuarm64"
DISTRO = "poky"
DISTRO_VERSION = "3.0.4"
TUNE_FEATURES = "aarch64 armv8a crc"
TARGET_FPU = ""
meta
meta-poky
meta-yocto-bsp = "HEAD:f2eb22a8783f1eecf99bd4042695bab920eed00e"

Initialising tasks: 100% |##################################################################################################################################| Time: 0:00:01
Sstate summary: Wanted 873 Found 0 Missed 873 Current 19 (0% match, 2% complete)
NOTE: Executing Tasks
NOTE: Setscene tasks completed
WARNING: unifdef-native-2.11-r0 do_fetch: Failed to fetch URL http://dotat.at/prog/unifdef/unifdef-2.11.tar.xz, attempting MIRRORS if available
WARNING: libtirpc-native-1.1.4-r0 do_fetch: Failed to fetch URL https://downloads.sourceforge.net/libtirpc/libtirpc-1.1.4.tar.bz2, attempting MIRRORS if available
WARNING: libcap-ng-native-0.7.9-r0 do_fetch: Failed to fetch URL http://people.redhat.com/sgrubb/libcap-ng/libcap-ng-0.7.9.tar.gz, attempting MIRRORS if available
ERROR: libtirpc-native-1.1.4-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1010/bus"; export PATH="/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/yocto-poky/scripts/native-intercept:/home/chunxi/yoctobuild/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/yocto-poky/scripts:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/usr/bin:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/usr/sbin:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/usr/bin:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/sbin:/home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/recipe-sysroot-native/bin:/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/yocto-poky/bitbake/bin:/home/chunxi/yoctobuild/tmp/hosttools"; export HOME="/home/chunxi"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/chunxi/yoctobuild/downloads 'https://downloads.sourceforge.net/libtirpc/libtirpc-1.1.4.tar.bz2' --progress=dot -v failed with exit code 4, output:
--2021-07-27 09:27:18-- https://downloads.sourceforge.net/libtirpc/libtirpc-1.1.4.tar.bz2
Resolving downloads.sourceforge.net (downloads.sourceforge.net)... failed: Name or service not known.
wget: unable to resolve host address ‘downloads.sourceforge.net’

ERROR: libtirpc-native-1.1.4-r0 do_fetch: Fetcher failure for URL: 'https://downloads.sourceforge.net/libtirpc/libtirpc-1.1.4.tar.bz2'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/chunxi/yoctobuild/tmp/work/x86_64-linux/libtirpc-native/1.1.4-r0/temp/log.do_fetch.21744
ERROR: Task (virtual:native:/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/yocto-poky/meta/recipes-extended/libtirpc/libtirpc_1.1.4.bb:do_fetch) failed with exit code '1'
WARNING: util-linux-native-2.34-r0 do_fetch: Failed to fetch URL https://cdn.kernel.org/pub/linux/utils/util-linux/v2.34/util-linux-2.34.tar.xz, attempting MIRRORS if available
NOTE: Tasks Summary: Attempted 227 tasks of which 157 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
virtual:native:/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/yocto-poky/meta/recipes-extended/libtirpc/libtirpc_1.1.4.bb:do_fetch

0 件の賞賛
返信
6,126件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please configure agent on your build host to make it possible to run the following command

wget https://downloads.sourceforge.net/libtirpc/libtirpc-1.1.4.tar.bz2

0 件の賞賛
返信
6,120件の閲覧回数
muaxi8
Contributor V

can you give me a yocto-based tiny userland file?

0 件の賞賛
返信
6,115件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
6,109件の閲覧回数
muaxi8
Contributor V

i can not access https://www.nxp.com/lgfiles/sdk/lsdk2012/rootfs_lsdk2012_yocto_tiny_arm64.tgz

muaxi8_1-1627460286839.png

 

 

muaxi8_0-1627460034460.png

google drive also can access.

can you send it to my e-mail address: [email protected]

or upload to the baidu  cloud  

0 件の賞賛
返信
6,107件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
4,313件の閲覧回数
zhan3
Contributor I
link is out of time,could you upload again?
0 件の賞賛
返信