The actual driver has support for the HS400 mode.
Please use the LLDP 6.1.55, with this one you don't have to add any patch driver or modify the dts.
please note:
root@localhost:~# cat /sys/kernel/debug/mmc1/ios
clock: 200000000 Hz
actual clock: 150000000 Hz
vdd: 21 (3.3 ~ 3.4 V)
bus mode: 2 (push-pull)
chip select: 0 (don't care)
power mode: 2 (on)
bus width: 3 (8 bits)
timing spec: 10 (mmc HS400)
signal voltage: 1 (1.80 V)
driver type: 0 (driver type B)
Technical parameters of the eSDHC HS400 mode are provided in the QorIQ LS1028A/LS1018A Data Sheet.
Due to A-011334: Limited clock dividers for HS400 mode, maximum SDHC_CLK frequency supported in HS400 (VDD=1.0v) mode is 150 MHz.