eMMC and LS1046a hardware design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC and LS1046a hardware design

2,131件の閲覧回数
Ellu24
Contributor III

Hello

I am doing a new hardware design using ls1046a and now trying to interface eMMC. I have some doubts regarding this.

1) I am planning to use emmc version 5.1 and whether it is supported by  processor or not.

2) to which pin of the processor hardware reset and RCLK of the emmc should connect.

0 件の賞賛
返信
3 返答(返信)

2,103件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

1. Please take a look at sections 19.1.1 and 19.1.2 of the LS1046A Ref Manual, these list  features and protocols supported by the processor. It can work with eMMC 5.1 devices, but supports only eMMC 4.5 features.

2. Please refer to https://www.nxp.com.cn/docs/en/application-note/AN5252.pdf

0 件の賞賛
返信

2,100件の閲覧回数
Ellu24
Contributor III

Thanks for the reply. can you please suggest me, where to connect the hardware reset of eMMC.

0 件の賞賛
返信

2,059件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "5.6.1 eSDHC pin termination recommendations" in AN5252.pdf.

0 件の賞賛
返信