dpdk-19.11+20.12 Compilation issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dpdk-19.11+20.12 Compilation issue

1,424件の閲覧回数
Subhani7
Contributor II

Hi Team,

I am using LLDPUG
Layerscape Linux Distribution POC User Guide

when I am downgrading dpdk version from 21.11 to 19.11, I am facing below issue .

ERROR: fsl-image-networking-1.0-r0 do_rootfs: Could not invoke dnf. Command '/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/recipe-sysroot-native/usr/bin/dnf -v --rpmverbosity=info -y -c /home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/rootfs/etc/yum.repos.d --installroot=/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/rootfs --setopt=logdir=/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/temp --repofrompath=oe-repo,/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/oe-rootfs-repo --nogpgcheck install base-passwd boost cronie curl dhcp-client dpdk glibc gps-utils gpsd i2c-tools icu kexec-tools ldd libbsd libbsd-dev libcurl libedit libpcap libsdl2 libssh2 libssl libunwind libusb1 libxml-parser-perl libxml2 linux-libc-headers-dev lksctp-tools logrotate lsb-release networkmanager networkmanager-bash-completion networkmanager-nmtui ntp openssl packagegroup-core-boot packagegroup-core-ssh-openssh packagegroup-fsl-benchmark-core packagegroup-fsl-mfgtools packagegroup-fsl-networking-core packagegroup-fsl-tools-core pciutils perl qcom-apps rpm rsyslog run-postinsts shadow tcpdump udev-extraconf udev-rules-qoriq usbutils vim zlib' returned 1:
DNF version: 4.11.1
cachedir: /home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/rootfs/var/cache/dnf
Added oe-repo repo from /home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/oe-rootfs-repo
User-Agent: falling back to 'libdnf': could not detect OS or basearch
repo: using cache for: oe-repo
oe-repo: using metadata from Tue 26 Mar 2024 05:34:19 AM UTC.
Last metadata expiration check: 0:00:01 ago on Tue 26 Mar 2024 05:36:48 AM UTC.
--> Starting dependency resolution
--> Finished dependency resolution
Error:
Problem: conflicting requests
- nothing provides kernel-module-rte-kni-5.10.35-rt39 needed by dpdk-19.11+20.12-r0.lx2160ardb_rev2
(try to add '--skip-broken' to skip uninstallable packages)

ERROR: Logfile of failure stored in: /home/labuser/NEERAJ/LLDP/LINUX/target/yocto/build_lx2160ardb-rev2/tmp/work/lx2160ardb_rev2-fsl-linux/fsl-image-networking/1.0-r0/temp/log.do_rootfs.1073
ERROR: Task (/home/labuser/NEERAJ/LLDP/LINUX/target/yocto/sources/meta-qoriq/recipes-fsl/images/fsl-image-networking.bb:do_rootfs) failed with exit code '1'

Can you please provide me some solution

0 件の賞賛
返信
1 返信

1,355件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use the default DPDK provided in LLDPUG release.

Please use the lower version LSDK, if you want to use DPDK 19.11.

 

0 件の賞賛
返信