dpaa2_ethsw dpsw.0: dpsw_reset err -5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dpaa2_ethsw dpsw.0: dpsw_reset err -5

2,012件の閲覧回数
156614400
Contributor III

1  I define the dpsw in the DPL file,   sometimes our new board start truely,  but sometimes start with error , error  is "dpaa2_ethsw dpsw.0: dpsw_reset err -5".

2 when start with error,  the DPMAC of DPSW  all are down,  and only one eth.

3 attachfile log1 is to start truely, log2 is to error of start 

0 件の賞賛
返信
3 返答(返信)

2,003件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached DPL configuration file using DPSW, please modify DPMAC definition in the attached file according to your custom board configuration.

タグ(1)
0 件の賞賛
返信

1,993件の閲覧回数
156614400
Contributor III

also same condition....attach file is my new dpl..

also sometimes dpsw init with err....

0 件の賞賛
返信

1,988件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached dpl file, which I have verified on lx2160ardb.

root@TinyLinux:~# dmesg | grep dpsw
[ 5.223834] dpaa2_ethsw dpsw.0: Adding to iommu group 2
[ 5.830439] dpaa2_ethsw dpsw.0: probed 4 port switch

0 件の賞賛
返信