dpaa2_ethsw dpsw.0: dpsw_reset err -5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dpaa2_ethsw dpsw.0: dpsw_reset err -5

2,007 Views
156614400
Contributor III

1  I define the dpsw in the DPL file,   sometimes our new board start truely,  but sometimes start with error , error  is "dpaa2_ethsw dpsw.0: dpsw_reset err -5".

2 when start with error,  the DPMAC of DPSW  all are down,  and only one eth.

3 attachfile log1 is to start truely, log2 is to error of start 

0 Kudos
Reply
3 Replies

1,998 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached DPL configuration file using DPSW, please modify DPMAC definition in the attached file according to your custom board configuration.

Tags (1)
0 Kudos
Reply

1,988 Views
156614400
Contributor III

also same condition....attach file is my new dpl..

also sometimes dpsw init with err....

0 Kudos
Reply

1,983 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached dpl file, which I have verified on lx2160ardb.

root@TinyLinux:~# dmesg | grep dpsw
[ 5.223834] dpaa2_ethsw dpsw.0: Adding to iommu group 2
[ 5.830439] dpaa2_ethsw dpsw.0: probed 4 port switch

0 Kudos
Reply