branches in yocto not syncing.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

branches in yocto not syncing.

941件の閲覧回数
gfine1
Contributor III

We had the need to rebuild our source trees as some changes were not getting picked up. 

In the shift to github from codeaurora it seems branches no longer exist in either

Linux source code migration (CAF -> Github) - NXP Community

or using 

repo init -u https://github.com/nxp-qoriq/yocto-sdk -b dunfell

During the repo sync we get this error.

gfine@LinuxServer:~/ls1043a_051723b$ repo init -u https://github.com/nxp-qoriq/yocto-sdk -b dunfell
Downloading Repo source from https://gerrit.googlesource.com/git-repo
remote: Counting objects: 151, done
remote: Finding sources: 100% (9/9)
remote: Total 9 (delta 4), reused 7 (delta 4)
Unpacking objects: 100% (9/9), done.

Your identity is: Glen Fine <[email protected]>
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/gfine/ls1043a_051723b
gfine@LinuxServer:~/ls1043a_051723b$ repo sync
remote: Enumerating objects: 147, done.
remote: Counting objects: 100% (147/147), done.
remote: Compressing objects: 100% (86/86), done.
remote: Total 134 (delta 71), reused 107 (delta 44), pack-reused 0
Receiving objects: 100% (134/134), 119.23 KiB | 38.00 KiB/s, done.
Resolving deltas: 100% (71/71), completed with 7 local objects.
Fetching: 50% (6/12) 6:44 | Last synced: openembedded/meta-openembeddedb' % Total % Received % Xferd Average Speed Time Time Time Current\n Dload Upload Total Spent Left Speed\n\r 0 0 0 0 0 0 0 0 --:--:-- --:--:-- --:--:-- 0curl: (6) Could not resolve host: source.codeaurora.org\n'
Fetching: 50% (6/12) 6:48 | Last synced: openembedded/meta-openembedded
fatal: unable to access 'https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq/': Could not resolve host: source.codeaurora.org

qoriq/qoriq-components/meta-qoriq:
fatal: unable to access 'https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq/': Could not resolve host: source.codeaurora.org
qoriq/qoriq-components/meta-qoriq: sleeping 4.0 seconds before retrying
fatal: unable to access 'https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq/': Could not resolve host: source.codeaurora.org

qoriq/qoriq-components/meta-qoriq:
fatal: unable to access 'https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq/': Could not resolve host: source.codeaurora.org
error: Cannot fetch qoriq/qoriq-components/meta-qoriq from https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq
Fetching: 75% (9/12) 6:54 | Last synced: meta-selinux

It seems dunfell is not longer available so we tried

repo init -u https://github.com/nxp-qoriq/yocto-sdk -b hardknott

and

repo init -u https://github.com/nxp-qoriq/yocto-sdk -b langfell

with the same result. 

I have combed the community to see if an update was posted.  

Are we working with the wrong repo? If so, what is the correct repo? We tried 

repo init -u https://github.com/nxp-imx/imx-manifest -b dunfell

and it failed as well.

 

 

0 件の賞賛
返信
0 返答(返信)