Write new rcw binary on the sd card image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write new rcw binary on the sd card image

1,574 Views
SoccerMom
Contributor II

Hello,

I have an LS1028ardb board with LSDK21.08. I boot it from the SD card using firmware_ls1028ardb_sdboot.img. I have modified the RCW for that LSDK and converted it to binary format. How can I write over this new rcw binary on the firmware_ls1028ardb_sdboot.img?

Thanks

0 Kudos
Reply
2 Replies

1,546 Views
June_Lu
NXP TechSupport
NXP TechSupport

Confirm the */flexbuild_lsdk2108/configs/board/ls1028ardb/manifest select rcw_sd,

rcw_sd="path/*.bin"(make sure the path is the required bin file)

$ cd flexbuild_lsdk2108/

$ source setup.env

$ flex-builder -i clean-firmware

$ flex-builder -c atf -m ls1028ardb -b sd

$ flex-builder -i mkfw -m ls1028ardb -b sd

Now the required image is available in*/flexbuild_lsdk2108/build/images

__________________________

Confirm the */flexbuild_lsdk2108/configs/board/ls1028ardb/manifest select rcw_xspi, rcw_xspi="path/*.bin"(make sure the path is the required bin file)

 

  1. $ cd flexbuild_lsdk2108/
  2. $ source setup.env
  3. $ flex-builder -i clean-firmware
  4. $ flex-builder -c atf -m ls1028ardb -b xspi
  1. $ flex-builder -i mkfw -m ls1028ardb -b xspi

Now the required image is available in*/flexbuild_lsdk2108/build/images

0 Kudos
Reply

1,567 Views
SoccerMom
Contributor II

I also tried to boot lsdk21.08 from NOR flash and then imported the original_rcw.bin in the PBL tool and just changed a field for GPIO and tried to write over the modified_rcw.bin in the NOR and boot up again. It does not not work, it does not transmit anything on the serial port.

 

originial_rcw.bin

original_rcw.png

 

modified_rcw.bin

modified_rcw.png

 

 

 

Thanks

0 Kudos
Reply