Without SEC enabled, is Secure Boot possible with the LS1021A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Without SEC enabled, is Secure Boot possible with the LS1021A?

1,631 Views
Karlito
Contributor I

Hi, I am currently using an NXP ls1021A and would like to implement Secure Boot. Is this possible without the Security Engine (SEC) enabled? Or is the implementation of Secure Boot only possible in combination with the use of the Security Engine?

@Layerscape® 1021A | NXP Semiconductors

0 Kudos
Reply
2 Replies

1,620 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

SEC disabled Layerscape chips cannot perform secure boot, the security engine (SEC 5.5) is designed to support Secure Boot.

Have a nice day!

Oswaldo.

 

0 Kudos
Reply

1,318 Views
Karlito
Contributor I

Thank you for your reply. Where can I find information on implementing Secure Boot with the LS1021A? Is there a step-by-step guide? I also want to know what is part of the SEC? Is the SFP module part of the SEC? Thanks in advance.

LS1021A 

Tags (2)
0 Kudos
Reply