What this PBI means?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What this PBI means?

3,576件の閲覧回数
2838219522
Contributor III

ufedor‌

I have a question.

In the AN5089.pdf.It said as below:

pastedImage_1.png

I shell with "md.b 60000000 80" in norflash bank0.display as below.

09 ee 02 00 60 10 00 00       I can understand this .Because location of u-boot in bank0 is at 0x60100000

 

I shell with "md.b 64000000 80" in norflash bank1.display as below.

09 ee 02 00 60 10 00 00       I can't understand this.The location of u-boot in bank1 is at 0x64100000.Why this PBI don't be 09 ee 02 00 64 10 00 00?

 

And it can boot from bank1 as well.

It's confused.

May I have your help,please?

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,316件の閲覧回数
ufedor
NXP Employee
NXP Employee

> The location of u-boot in bank1 is at 0x64100000.

The CPLD on the LS1021A-TWR board can be used to divide the NOR flash into two banks.

Please read the mentioned AN, 3 Copying the RCW and U-Boot into the upper bank.

0 件の賞賛
返信

3,316件の閲覧回数
2838219522
Contributor III

So ,you mean that the CPLD will map 0x64000000 and 0x64100000 to 0x60000000 and 0x60100000 when the board boots from bank1 .

0 件の賞賛
返信

3,316件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes.

3,316件の閲覧回数
2838219522
Contributor III

Thank you ,man.

0 件の賞賛
返信