Watchdog timer for LX2160A - reset identification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog timer for LX2160A - reset identification

1,463件の閲覧回数
anjana1
Contributor I

Hi

I am working with LX2160A processor and SDK 20.12. when the watchdog timer is about to reset, is there any application or any other way to identify that the reset is due to this?

Thanks in advance.

0 件の賞賛
返信
1 返信

1,431件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The RSTRQSR contains status bits to record the reasons for RESET_REQ_B assertion. The bits here are set independent of the RSTRQMR. This means if a reset occurs and is masked by RSTRQMR, it will still be recoreded in RSTRQSR. Excludes core watchdog timer sources ).

yipingwang_0-1691656079745.png

TrustZone WDOG second timeout goes to HREST_REQ

 

0 件の賞賛
返信