WDI PIN OF PF8100 TO LS1046

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WDI PIN OF PF8100 TO LS1046

1,949 Views
Ellu24
Contributor III

To which pin of LS1046 I should connect WDI pin of PF8100 PMIC, if I want to enable WD reset? 

Please find PF8100 datasheet. 

Thanks in advance

0 Kudos
Reply
1 Reply

1,937 Views
yipingwang
NXP TechSupport
NXP TechSupport

To enable WD reset, connect the pin to HRESET of LS1046A.
Required input assertion time of HRESET_B is 32 SYSCLKs.
Customer has to keep in mind the following when enabling WD reset.
1. If min. assertion time of WD pin is greater than min. assertion time of HRESET then WD reset will be successful.
2. If WD reset is configurable then change the min assertion time of WDI pin as per the requirement based on HRESET.
3. If WD reset is not configurable the use Reset IC in between.

0 Kudos
Reply