Ubuntu Server on LS2088A based board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ubuntu Server on LS2088A based board

1,360件の閲覧回数
suryaprakash_ra
Contributor I

I am looking for a support to run "Ubuntu Server" on LS2088A based board. From Auto_Linux_BSP_18.0_BlueBox_Quick_Start.pdf, it is observed that "ubuntu base" is supported in NXP BlueBox. My use case is to run the "Ubuntu Server" on LS2088A base board.  Please provide me some reference and procedure to install ubuntu server and proceed further.

ラベル(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
bpe
NXP Employee
NXP Employee

 I think, the simplest way to achieve that is to install the base as
 specified in the BSP documentation and use aptitude or another
 package manager to add the "server" task group.
 
 If you are looking for ready detailed guides on how to start Ubuntu server
 right from the SDK, I'm afraid, none is  available.
 
 


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信