Ubuntu Server on LS2088A based board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ubuntu Server on LS2088A based board

1,001 次查看
suryaprakash_ra
Contributor I

I am looking for a support to run "Ubuntu Server" on LS2088A based board. From Auto_Linux_BSP_18.0_BlueBox_Quick_Start.pdf, it is observed that "ubuntu base" is supported in NXP BlueBox. My use case is to run the "Ubuntu Server" on LS2088A base board.  Please provide me some reference and procedure to install ubuntu server and proceed further.

标签 (1)
0 项奖励
回复
1 回复

868 次查看
bpe
NXP Employee
NXP Employee

 I think, the simplest way to achieve that is to install the base as
 specified in the BSP documentation and use aptitude or another
 package manager to add the "server" task group.
 
 If you are looking for ready detailed guides on how to start Ubuntu server
 right from the SDK, I'm afraid, none is  available.
 
 


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复