Uboot debugging in code warrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Uboot debugging in code warrior

2,326件の閲覧回数
rashmikj
Contributor III

I am trying to debug uboot using code warrior in LS1046ardb Kit. I followed the steps mentioned in CodeWarrior for ARMv8 Using in u.pdf.

It always stops at Break at address "0x100000d0" with no debug information available, or outside of program code.

When i fuse the corresponding fip_uboot.bin file in qspi flash , uboot comes up and i can see in uart logs.

0 件の賞賛
返信
1 返信

2,300件の閲覧回数
Pavel
NXP Employee
NXP Employee

Do you use the AN4876 for u-boot debugging? See the following document:

https://www.nxp.com/docs/en/application-note/AN4876.pdf

0 件の賞賛
返信