USB not detected LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB not detected LS1043ARDB

5,580件の閲覧回数
bladerunner1010
Contributor III

??

0 件の賞賛
返信
5 返答(返信)

5,494件の閲覧回数
bladerunner1010
Contributor III

Any ideas appreciated 

Thanks

 

0 件の賞賛
返信

5,485件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

I deployed the same SD boot environment, however still cannot reproduce your problem.

 

Do you use USB Mass Storage device? 

You could try whether USB could be detected when using ubuntu main rootfs. As normal rootfs filesystem should not be the root cause.

0 件の賞賛
返信

5,532件の閲覧回数
bladerunner1010
Contributor III

?

0 件の賞賛
返信

5,514件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Have your modified dts or Kernel configuration file?

If yes, please use boot_LS_arm64_lts_5.10.tgz which I specified.

0 件の賞賛
返信

5,541件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download LSDK 21.08 bootpartition tar ball with the following command.

wget https://www.nxp.com/lgfiles/sdk/lsdk2108/boot_LS_arm64_lts_5.10.tgz

Then use Image and fsl-ls1043a-rdb-sdk.dtb from that tar all.

As normally, this problem should not be related with rootfs filesystem.

Please refer to my attached console log, there is no problem to use USB device in the Tiny Buildroot rootfs.

0 件の賞賛
返信