Time Synchronization using GPS (LS1046/LS1088)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Time Synchronization using GPS (LS1046/LS1088)

4,488 Views
muhammed_mufeed
Contributor I

Hi,
I know how to synchronize time using IEEE1588 (PTP). How can I Synchronize Internal clock of LS1046/LS1088 with GPS time. As per my knowledge for synchronizing a system with GPS we need ToD information and 1PPS signal from GPS receiver. I can connect GPS via UART to LS1046/LS1088. But where I connect 1PPS signal?

Labels (1)
0 Kudos
Reply
6 Replies

4,327 Views
kien_tran
Contributor II

Hi ufedor‌

Once a 1 PPS is connected to the TMR_TRIG1 input, does the times tamping engine automatically adjust it's time to the 1 PPS?

-Kien

0 Kudos
Reply

4,327 Views
muhammed_mufeed
Contributor I

Hi Fedor,

To implement PTP master. A PTP master contains a gps receiver to get UTC time. GPS receiver will provide ToD information and 1PPS signal to synchronize PTP master with UTC.

0 Kudos
Reply

4,327 Views
muhammed_mufeed
Contributor I

Hi Ufedor,

Can I phase align my 1588 nominal clock with this 1PPS input connected to the  TMR_TRIG1 input.

0 Kudos
Reply

4,327 Views
ufedor
NXP Employee
NXP Employee

Not clear what do you mean and why it can be needed.

0 Kudos
Reply

4,327 Views
ufedor
NXP Employee
NXP Employee

The 1 PPS signal has to be connected to the TMR_TRIG1 input.

0 Kudos
Reply

3,548 Views
hmz-rhl
Contributor I
is it the same for LS1043 ? and what did you mean by "connect" pls
0 Kudos
Reply