Temperature sensor on LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature sensor on LS1043ARDB

ソリューションへジャンプ
2,435件の閲覧回数
ts1234
Contributor III

Is there any temperature sensor available on LS1043ARDB?

 

0 件の賞賛
返信
1 解決策
2,428件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Design Board Reference Manual, 4.4 Temperature anode and cathode:

"The LS1043ARDB has two pins, TD1_Anode and TD1_Cathode. These pins are connected to a thermal body diode on the die that allows direct temperature measurement. The pins are connected to an SA56004ED device (U45) with dual-channel thermal monitor. This allows you to take direct die temperature readings with an accuracy of ±1 °C."

元の投稿で解決策を見る

2 返答(返信)
2,417件の閲覧回数
ts1234
Contributor III

I have tried lm-sensors to check the temperature. No external device is connected to LS1043ARDB.

Why do I see a high value on temp2?

root@localhost:~# sensors
adt7461-i2c-0-4c
Adapter: 2180000.i2c
temp1: +59.0 C (low = +0.0 C, high = +70.0 C)
(crit = +85.0 C, hyst = +75.0 C)
temp2: +76.1 C (low = +0.0 C, high = +70.0 C) ALARM (HIGH)
(crit = +85.0 C, hyst = +75.0 C)

root@localhost:~#

0 件の賞賛
返信
2,429件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Design Board Reference Manual, 4.4 Temperature anode and cathode:

"The LS1043ARDB has two pins, TD1_Anode and TD1_Cathode. These pins are connected to a thermal body diode on the die that allows direct temperature measurement. The pins are connected to an SA56004ED device (U45) with dual-channel thermal monitor. This allows you to take direct die temperature readings with an accuracy of ±1 °C."