Switch Setup on LS1028ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Switch Setup on LS1028ARDB

19,486件の閲覧回数
zing
Contributor II

Hi

I try to get the interfaces swp0-swp3 to run. I use the following software

root@LS1028ARDB-Ubuntu:~# uname -a
Linux LS1028ARDB-Ubuntu 5.4.3-rt1 #1 SMP PREEMPT_RT Wed May 27 07:13:13 CEST 2020 aarch64 aarch64 aarch64 GNU/Linux

The following release was used to build the os:

OpenIL-v1.8-202005

I try to setup the switch interfaces as described in LSDKUG_Rev19.09 Figure 211. The output of the given script is:

setup_bridge.sh  setup_eno0.sh    setup_switch.sh  
root@LS1028ARDB-Ubuntu:~# ./setup_switch.sh
RTNETLINK answers: Network is down
RTNETLINK answers: Network is down
RTNETLINK answers: Network is down
RTNETLINK answers: Network is down
ls: cannot access '/sys/bus/pci/devices/0000:00:00.6/net/': No such file or directory
Not enough information: "dev" argument is required.

Also i can not bring the interfaces up manually (eno0 works fine dhc and everything works!)

I suspect a driver problem, however it seem the felix driver is there:

root@LS1028ARDB-Ubuntu:~# dmesg | grep "felix"                                                                                      
[    2.966984] mscc_felix 0000:00:00.5: Adding to iommu group 1
[    2.967221] mscc_felix 0000:00:00.5: Failed to register DSA switch: -517
[    3.467052] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 0
[    3.467337] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 1
[    3.467610] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 2
[    3.467882] mscc_felix 0000:00:00.5: Found PCS at internal MDIO address 3
[    3.728010] mscc_felix 0000:00:00.5 swp0 (uninitialized): PHY [0000:00:00.3:10] driver [Microsemi GE VSC8514 SyncE]
[    3.967994] mscc_felix 0000:00:00.5 swp1 (uninitialized): PHY [0000:00:00.3:11] driver [Microsemi GE VSC8514 SyncE]
[    4.207994] mscc_felix 0000:00:00.5 swp2 (uninitialized): PHY [0000:00:00.3:12] driver [Microsemi GE VSC8514 SyncE]
[    4.455995] mscc_felix 0000:00:00.5 swp3 (uninitialized): PHY [0000:00:00.3:13] driver [Microsemi GE VSC8514 SyncE]
[    4.456423] mscc_felix 0000:00:00.5: configuring for fixed/internal link mode
[    4.456447] mscc_felix 0000:00:00.5: Link is Up - 2.5Gbps/Full - flow control off
root@LS1028ARDB-Ubuntu:~#

Any Ideas how to bring up the switch interfaces?

ラベル(1)
5 返答(返信)

19,345件の閲覧回数
sameer_chouksey
Contributor II

Hello [email protected],

I am facing a similar issue. Can you please share setup_bridge.sh, setup_eno0.sh and setup_switch.sh files?

Regards,

Sameer

0 件の賞賛
返信

19,340件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached script and the following test procedure.

root@ls1028ardb:~# bash +x enetc_switch_cpu_port_without_bridge_dsa.sh
[ 79.858412] Generic PHY fixed-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=fixed-0:00, irq=POLL)
[ 79.869942] fsl_enetc 0000:00:00.2 eno2: Link is Up - 1Gbps/Full - flow control off
[ 79.875622] 8021q: adding VLAN 0 to HW filter on device eno2
[ 79.883568] IPv6: ADDRCONF(NETDEV_CHANGE): eno2: link becomes ready
[ 79.890333] mscc_felix 0000:00:00.5 swp0: configuring for inband/qsgmii link mode
[ 79.898883] 8021q: adding VLAN 0 to HW filter on device swp0
[ 79.907080] mscc_felix 0000:00:00.5 swp1: configuring for inband/qsgmii link mode
[ 79.915531] 8021q: adding VLAN 0 to HW filter on device swp1
[ 79.923639] mscc_felix 0000:00:00.5 swp2: configuring for inband/qsgmii link mode
[ 79.932112] 8021q: adding VLAN 0 to HW filter on device swp2
[ 79.940204] mscc_felix 0000:00:00.5 swp3: configuring for inband/qsgmii link mode
[ 79.948625] 8021q: adding VLAN 0 to HW filter on device swp3
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# ifconfig swp0 down
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# ifconfig swp0 100.1.1.29 netmask 255.255.255.0
[ 90.042476] mscc_felix 0000:00:00.5 swp0: configuring for inband/qsgmii link mode
[ 90.050569] 8021q: adding VLAN 0 to HW filter on device swp0
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# [ 93.131335] mscc_felix 0000:00:00.5 swp0: Link is Up - 1Gbps/Full - flow control off
[ 93.139218] IPv6: ADDRCONF(NETDEV_CHANGE): swp0: link becomes ready
ifconfig swp0 up
root@ls1028ardb:~# echo $?
0
root@ls1028ardb:~# ping -c 5 -s 1 100.1.1.1
PING 100.1.1.1 (100.1.1.1) 1(29) bytes of data.
9 bytes from 100.1.1.1: icmp_seq=1 ttl=64
9 bytes from 100.1.1.1: icmp_seq=2 ttl=64
9 bytes from 100.1.1.1: icmp_seq=3 ttl=64
9 bytes from 100.1.1.1: icmp_seq=4 ttl=64
9 bytes from 100.1.1.1: icmp_seq=5 ttl=64

--- 100.1.1.1 ping statistics ---
5 packets transmitted, 5 received, 0% packet loss, time 4081ms

3,510件の閲覧回数
noahw
Contributor III

I am trying to set up ethernet interface on LS1028ARDB as well. I run your shell script to bring the interfaces up, then follow the next steps. I do see the lines:

mscc_felix 0000:00:00.5 swp0: Link is Up -- 1Gbps/Full - flow control rx/tx

IPv6: ADDRCONF(NETDEV_CHANGE): swp0: link becomes ready

 

However, when I try ping -c 5 -s 1 100.1.1.1, the ping fails and I get Destination Host Unreachable.

my output of `ip a` shows:

eno2: <BROADCAST,MULTICAST,UP,LOWER_UP> with no ip address, and

swp0@eno2: <BROADCAST,MULTICAST,UP,LOWER_UP> with ip address 100.1.1.29

 

Any ideas?

タグ(1)
0 件の賞賛
返信

19,009件の閲覧回数
xuchegndi
Contributor II

Hi Sir, I am using LS1028A board,

how can I print the debug message as follows when using 'ifconfig' :

root@ls1028ardb:~# ifconfig swp0 100.1.1.29 netmask 255.255.255.0
[ 90.042476] mscc_felix 0000:00:00.5 swp0: configuring for inband/qsgmii link mode
[ 90.050569] 8021q: adding VLAN 0 to HW filter on device swp0

0 件の賞賛
返信

19,340件の閲覧回数
zing
Contributor II

Thanks for your response and adjusted script! Interfaces are now up and I can use them.

0 件の賞賛
返信