Security Engine of LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Security Engine of LS1021A

2,085 Views
tecuelee
Contributor I

I am currently being developed based on LS1021A-IoT.
I have a difficulty with respect to Security engine.
I try to change the api using security engine instead using S/W openssl.
It applied as follows, but there is little change in speed.

root@OpenWrt:/# modprobe cryptodev
[             ] cryptodev: driver 1.8 loaded
root@OpenWrt:/# openssl engine
(cryptodev) BSD cryptodev engine
(dynamic) Dynamic engine loading support

What went wrong? Or seek advice.

Labels (1)
0 Kudos
Reply
2 Replies

1,669 Views
bpe
NXP Employee
NXP Employee

Enabling cryptodev driver alone does not offload crypto jobs to the

hardware. You should also enable the hardware (CAAM in your case)

driver. Suggestions:

1. Use NXP QorIQ SDK:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

2. Follow the SDK documentation:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-70AB1917-E7BD-45DB-924C-7...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-FD8EAB86-C554-4D24-9B50-F...


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,669 Views
tecuelee
Contributor I

P{font-size:14px; line-height:16em; margin-left:0; margin-top:0;

margin-right:0; margin-bottom:0; font-family:맑은 고딕;}

Dear bpe

I thank you for your quick reply

My situation is the same

 

root@OpenWrt:/# modprobe cryptodev

cryptodev: driver 18 loaded

root@OpenWrt:/# openssl version

OpenSSL 101g 7 Apr 2014

root@OpenWrt:/# openssl engine

(cryptodev) BSD cryptodev engine

(dynamic) Dynamic engine loading support

root@OpenWrt:/# modprobe tcrypt

modprobe: FATAL: Module tcrypt not found

root@OpenWrt:/# grep tls /proc/crypto

name         :

tls10(hmac(sha1),cbc(aes))

driver       : tls10-hmac-sha1-cbc-aes-caam

root@OpenWrt:/# cat /proc/interrupts | grep -i qman

root@OpenWrt:/#

root@OpenWrt:/# cat /proc/interrupts | grep jr

135:         

2         

0       GIC 135  1710000jr

136:         

8         

0       GIC 136  1720000jr

137:         

0         

0       GIC 137  1730000jr

138:         

0         

0       GIC 138  1740000jr

 

How can I check the CAAM features on LS1021A-IoT platforms?

How can I use the Security engine acceleration with OpenSSL, cryptodev,

CAAM?

My company is a company that specializes in the development api

Perhaps, is there any sample application that can use CAAM features?

 

regards,

 

Tecue Lee

JEENWOO R&D Manager

 

0 Kudos
Reply