SError in LS1023A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SError in LS1023A

4,376 Views
Jason77
Contributor I

Hello,
We use LS1023a to develop the product.(kernel version:5.4.47)
After using the product for a while(few weeks), a kernel panic occurred.
The kernel panic information is "Kernel panic - not syncing: Asynchronous SError Interrupt".
ARM manual says "SError generation is IMPLEMENTATION DEFINED."
https://developer.arm.com/documentation/102412/0103/Exception-types/Asynchronous-exceptions
Could NXP provide all LS1023a's SError generation reasons?
We need to investigate Serror root cause for this issue.
Thanks

Labels (1)
0 Kudos
Reply
5 Replies

4,347 Views
yipingwang
NXP TechSupport
NXP TechSupport

Which component caused the SError? PCIe, DPAA Ethernet?

Would you please provide the whole Linux Kernel panic console log?

0 Kudos
Reply

4,332 Views
Jason77
Contributor I

Thanks, you for help.

We do not know which component cause this issue.

It happens suddenly after a long time.

CPU receive/transmit data from DDR, PCIE, ethernet, emmc, uart in the background.

So, we would like to know about LS1023a's SError generation reasons (IMPLEMENTATION DEFINED by NXP).

We will check one by one.

The attached file is panic information.

Could you provide" SError generation" information for our reference?

Thanks

0 Kudos
Reply

4,171 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

I did not see specific SError definitions for LS1023a.


Customer can check ESR_ELx.IDS to get to know whether they are IMPLEMENTATION DEFINED SErrors, and check ESR to get more error info.

0 Kudos
Reply

4,155 Views
Jason77
Contributor I
Thanks you, we will check ESR_ELx.IDS first.
0 Kudos
Reply

4,263 Views
yipingwang
NXP TechSupport
NXP TechSupport

Confirming with the AE team now.

0 Kudos
Reply