Raspberry pi operating system on layerscape

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Raspberry pi operating system on layerscape

1,253 Views
DMH
Contributor I

Hello there

I would like to run a raspberry pi image on a layerscape processor, for better performance and building a custom system that costs less. The application is a firewall for networks and running peer to peer VPN services.

I am not the greatest at building a custom rom or firmware but i want to use a firmware/rom already available.

I need to run the following: 3 Gigabit NIC's (ethernet); disk usage led; 2GB ram; 16GB boot drive; real time clock and video output with usb input for a keyboard

Thanks for reading      hope you can help.

0 Kudos
Reply
1 Reply

1,244 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

Sorry but that is not possible!

The images for Raspberry Pi are built for their processor and you can't run that OS on Layerscape processors.

You can install ubuntu on your Layers scape and try to install the same apps or similar to your application

0 Kudos
Reply