RGMII does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RGMII does not work

2,046件の閲覧回数
allan_yi
Contributor I

   hello

I Use LS1043+QCA8337 wiht SGMII ,but it does not work, The ping test failed.  so I want  to do loopback test about the bus of serdes,but I can not do the loopback test abou  serders Of lanA ,because the register of bit 3 can not write.could you give me some advices,or tell me how to do the loopback test thanks a lot!

pastedImage_1.png

=> mw.l 0x1ea083c 8
=> md.l 0x1ea083c 1
01ea083c: 00000004 ....
=> mw.l 0x1ea083c 5
=> md.l 0x1ea083c 1
01ea083c: 00000005 ....
=> mw.l 0x1ea083c 0xc
=> md.l 0x1ea083c 1
01ea083c: 00000004 ....
=> mw.l 0x1ea083c c
=> md.l 0x1ea083c 1
01ea083c: 00000004

pastedImage_3.png

pastedImage_4.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,955件の閲覧回数
ufedor
NXP Employee
NXP Employee

The "01b - Loopback Mode" corresponds to the bit value 0x10.

0 件の賞賛
返信

1,955件の閲覧回数
allan_yi
Contributor I

when I write 8 to this bit ,but it is fail.FYI 

pastedImage_1.png

0 件の賞賛
返信