Qbv not working (does not distinguish between traffic classes)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qbv not working (does not distinguish between traffic classes)

1,489 Views
ZippZapp
Contributor II

Hello,

I am struggling to get Qbv working as expected on bsp 0.3.

I have connected eno0 ("MAC0") of two LS1028A ARDB's and a linux PC together in a LAN (with a dumb switch), and established a VLAN 1 on all such that:

LS1028ARDB #1: eno0.1 has ip 195.168.1.1/24

LS1028ARDB #2: eno0.1 has ip 195.168.1.2/24

PC: eth0.1 has ip 195.168.1.3/24

vconfig set egress_map and vconfig_set_ingress_map has been run all all such that all traffic on the VLAN ends up with a VLAN priority of 4.

Pinging the PC from either LS1028ARDB confirms in wireshark on the PC that the ICMP request and reply packets do indeed have the correct VLAN ID and priority. Similarly tcpdump run on both LS1028ARDB's show that ICMP requests arrive with the correct VLAN ID and priority.

In addition all the above equipment can ping each other on a 10.0.1.0 net (no VLAN).

A qbv.txt file has been created with the following contents:

t0     00000000b     100000
t1     10111110b     1000000000

This has been entered into tsntool as such:

tsntool>qbvset --device eno0 --entryfile /qbv.txt

tsntool>qbvget --device eno0 confirms that setup has been set

(btw: doesn't work on switch ports).

With the above setup no traffic flows whatsoever. I would expect traffic to flow on my VLAN 1 with priority 4.

If it is changed to:

t0     00000001b     100000
t1     10111110b     1000000000

then traffic on all traffic classes flow - all with the same LOW bandwidth. I would expect VLAN 1 with priority 4 to have a much better bandwidth than traffic class 0.

If it is changed to:

t0     00000001b     1000000000
t1     10111110b     100000

then traffic on all traffic classes flow - all with the same HIGH bandwidth. I would expect VLAN 1 with priority 4 to have a much lower bandwidth than on traffic class 0.

All experimentation show far show that the switch does not distinguish between traffic classes at all. It behaves as if gate bit 0 and period in the qbv.txt file are the only values that matter. Gates bit 1-7 are don't-care.

What am I missing ?

Extremely grateful for any help ... please ...

Labels (1)
0 Replies