QSGMII interface not working, LS2085a Based Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSGMII interface not working, LS2085a Based Board

1,949 Views
jitenpatel
Contributor II

Hi all, I am using custom based board based on LS2085A QDS. We are using Serdes 1 protocol = 0x37.  The protocol sums up below:-

Serdes lanes:-

H

G

F

E

D

C

B

A

Serdes protocol

XFI1

XFI2

QSGMIIc

QSGMIId

PCIe2

From the above interfaces we are not using E lane (QSGMIId) . The QSGMIIc (F lane) signals are connected to Quad PHY IC (F104S8A) and four physical ports are brought out of the board.

For getting the QSGMIIc interface working we did the following changes:-

1) Selected 0x37 as serdes 1 protocol.

2) Flashed and Booted Management Complex firmware

3) Booted kernel, We are using EAR6 SDK

4) QSGMIIc uses MAC9 to MAC12 , therefore we created four PHY nodes in dts file and added this phy handle to corresponding MACs. 

But still our QSGMII interface doesn't seems to work. We are using LS2085aQDS kernel dts and dtsi file as our reference. Is there anything else we are missing from the above steps.

Can anyone validate our procedure or provide any steps for configuring QSGMII interface ?

Labels (1)
0 Kudos
Reply
1 Reply

1,757 Views
ufedor
NXP Employee
NXP Employee

Please check whether workaround for the erratum A-009442 is implemented.

Please consider creating a Technical Case if further support will be needed:

How I could create a Service Request? | NXP Community 

0 Kudos
Reply