QE / UCC UART on LS1088

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QE / UCC UART on LS1088

3,623件の閲覧回数
mcbridematt
Contributor III

I'm trying to see if I can use the QUICC Engine (QE) on the LS1088A to get two extra four wire UARTs.

I'm not getting any characters in or out of either UC1/UC3 TXD/RXD

So far I have:

  1. Set IRQ_EXT=2 so IRQ[3:9] is mapped to the UC1/UC3 UART functions
  2. Set IIC4_EXT=3 so IIC4 SDA/SCL is mapped to UC1/UC3 CDB (carrier detect).
    RCWSR12 reads back:
    md 1e0012C 1
    01e0012c: 02000600
  3. Added this to fsl-ls1088a.dtsi, based on the content of fsl-ls1043a.dtsi. I changed the clock and IRQ settings as appropriate:
    uqe: uqe@2400000 {
    	#address-cells = <1>;
    	#size-cells = <1>;
    	device_type = "qe";
    	compatible = "fsl,qe", "simple-bus";
    	ranges = <0x0 0x0 0x2400000 0x40000>;
    	reg = <0x0 0x2400000 0x0 0x480>;
    	brg-frequency = <150000000>; /* BRG is 1/2 of the QE bus frequency? */
    	bus-frequency = <350000000>; /* QE gets 1/2 of the platform clock 700MHz */
    	fsl,qe-num-riscs = <1>;
    	fsl,qe-num-snums = <28>;
    	status = "disabled";
    	qeic: qeic@80 {
    		compatible = "fsl,qe-ic";
    		reg = <0x80 0x80>;
    		#address-cells = <0>;
    		interrupt-controller;
    		#interrupt-cells = <1>;
    		interrupts = <GIC_SPI 96 IRQ_TYPE_LEVEL_HIGH>,
    			<GIC_SPI 96 IRQ_TYPE_LEVEL_HIGH>;
    	};
    	si1: si@700 {
    		#address-cells = <1>;
    		#size-cells = <0>;
    		compatible = "fsl,ls1043-qe-si",
    				"fsl,t1040-qe-si";
    		reg = <0x700 0x80>;
    	};
    	siram1: siram@1000 {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		compatible = "fsl,ls1043-qe-siram",
    				"fsl,t1040-qe-siram";
    		reg = <0x1000 0x800>;
    	};
    
    	ucc1: ucc@2000 {
    		cell-index = <1>;
    		reg = <0x2000 0x200>;
    		interrupts = <32>;
    		interrupt-parent = <&qeic>;
    	};
    
    	ucc3: ucc@2200 {
    		cell-index = <3>;
    		reg = <0x2200 0x200>;
    		interrupts = <34>;
    		interrupt-parent = <&qeic>;
    	};
    
    	muram@10000 {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		compatible = "fsl,qe-muram", "fsl,cpm-muram";
    		ranges = <0x0 0x10000 0x6000>;
    		data-only@0 {
    				compatible = "fsl,qe-muram-data",
    			"fsl,cpm-muram-data";
    				reg = <0x0 0x6000>;
    		};
    	};
    };
  4. Added this to my device DTS:
    &uqe {
    	status = "okay";
    	ucc@2000 {
    		device_type = "serial";
    		compatible = "ucc_uart";
    		rx-clock-name = "brg1";
    		tx-clock-name = "brg1";
    		port-number = <0>;
    	};
    	ucc@2200 {
    		device_type = "serial";
    		compatible = "ucc_uart";
    		rx-clock-name = "brg2";
    		tx-clock-name = "brg2";
    		port-number = <1>;
    	};
    };
  5. Configured U-Boot to load the QE firmware:
    Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0
    QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1
  6. Applied the patch soc: fsl: qe: convert QE interrupt controller to platform_device on top of my kernel 5.10.112

In my kernel log I see:

[    1.532562] 2402000.ucc: ttyQE0 at MMIO 0x2402000 (irq = 107, base_baud = 9375000) is a QE
[    1.540926] ucc_uart 2402000.ucc: UCC1 assigned to /dev/ttyQE0
[    1.546898] 2402200.ucc: ttyQE1 at MMIO 0x2402200 (irq = 108, base_baud = 9375000) is a QE
[    1.555261] ucc_uart 2402200.ucc: UCC3 assigned to /dev/ttyQE1

For testing I have made sure the flow control is "disabled":

  • Pulled CDB for both UCC's to GND
  • Pulled RTSB to GND

I can send characters to the ttyQEx and it doesn't freeze, so I assume the QE firmware is working:

# stty -F /dev/ttyQE0
speed 9600 baud; line = 0;
-brkint -imaxbel
# echo "test" > /dev/ttyQE0
# echo "test" > /dev/ttyQE1

I can't see any signal activity on any of the UCx pins when characters are sent, and if I try to send characters to the RXD pin I don't see it either.

Is there something I am missing?

ラベル(1)
タグ(4)
0 件の賞賛
返信
4 返答(返信)

3,557件の閲覧回数
mcbridematt
Contributor III

Still stuck on this.

I can verify that the uQE firmware has been loaded and is operational by reading out the microcode version register (CEURNR) and by checking the FLG semaphore after issuing QE commands.

I also configured BRGO2 to output on a pin and can see the output frequency about the same as the serial baud x16.

But:

  • I can't see any interrupts on the QE-IC (GIC 128)
  • In the UCC UART transmit sequence, the event and status register always read 0.

The lack of interrupts concern me the most, is there any easy way to cause a QE interrupt, preferably without any external pin output/input?

 

0 件の賞賛
返信

3,607件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In u-boot source code, please define the following options in  include/configs/ls1088a_common.h.

CONFIG_U_QE

CONFIG_SYS_QE_FW_ADDR

In board/freescale/ls1088a/ls1088a.c, please define the following.

#ifdef CONFIG_U_QE
u_qe_init();
#endif

Please refer to ls1043ardb as an example.

 

0 件の賞賛
返信

3,604件の閲覧回数
mcbridematt
Contributor III

As described above, I already modified my U-Boot to load the uQE binary.

Since my board is based on TF-A I changed U-Boot so I can supply the binary via the qe fw command which does:

qe_immr = (qe_map_t *)(CONFIG_SYS_IMMR + QE_IMMR_OFFSET);
if (!u_qe_upload_firmware((const struct qe_firmware *)addr)) {
	out_be32(<qe_immr->iram.iready, QE_IRAM_READY);
	return CMD_RET_SUCCESS;
}

Any idea if my device tree settings (particularly bus/clock) is correct?

I could not find any device tree for the LS1088A with the uQE defined, so I made a guess based on the content of LS1088ARM.

0 件の賞賛
返信

3,582件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

For UCC UART device tree definition, please refer to QE serial definition in arch/powerpc/boot/dts/fsl/p1025rdb.dtsi.

タグ(1)
0 件の賞賛
返信