Port pin status during RESET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port pin status during RESET

1,227 Views
FK
Contributor I

What is the port pin status of ball E13 "IFC_PAR1/GPIO2_14/QSPI_DIO_B1/FTM6_CH1", while LS1021A is set into RESET state?

Datasheet (Rev. 7, 06/2019) doesn't provide any notes for this pin. Is there any internal weak pull resistor applied or is the pin in high-z mode?

Labels (1)
0 Kudos
Reply
1 Reply

1,186 Views
ufedor
NXP Employee
NXP Employee

The pin is tri-stated when PORESET_B is asserted.

0 Kudos
Reply